BIOS version 5.20 for Satellite P70-B (PSPPNx)
- File: sppnv520.exe
- Version: 5.20
- Posted Date: 2015-11-11
- Release Date: 2015-10-29
- Other Versions
-
Release Date: Version: 2015-11-10 5.10 2014-12-10 1.10 2014-12-11 1.00
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
- The BIOS update will force the computer to shut down or restart. Please make sure to save all work in progress before starting BIOS updates.
- For CD-ROM BIOS updates: (1) Shut down the system while pressing the SHIFT key to completely power off. (2) Power on while pressing F2 to enter the BIOS Setup Menu. (3) From the Security tab and set the "Secure Boot" setting to "Disabled". (4) From the Advanced tab, enter "System Configuration" and set the Boot Mode to "CSM Boot" if the option is available. (5) Press F10 to save and exit. (6) Boot from the BIOS CD-ROM then type FLASH at the prompt. (7) After the BIOS update has completed, restore the BIOS settings that were changed.
- Note: The BIOS Launcher "CD_ROM Installation" option may not automatically proceed to burn the CD-ROM. If this occurs navigate to the root directory of the C-Drive then open the directory named after the BIOS filename (ex. C:\scqev520), then manually burn the CD-ROM from the disc image (ISO) file.
- After the BIOS update completes, power on the computer if it is off.
- While the "TOSHIBA" logo is displayed, press the F2 function key to start BIOS Setup.
- Check the version of BIOS, press the F9 function key then Enter to load setup defaults.
- Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.
Release Notes
Change History
- Version 5.20 - 2015-10-29
- Updated the Tropo Pro Video BIOS (VBIOS) to version to AB328832.bin.
- Updated the Microcode version to 0x1E.
- Added support for Windows 10.
- Added support for a new DMI Specification.
- Updated the Insyde code for an Intel S3 Security issue.
- Updated the Management Engine (ME) version to 9.1.30.1008 for the Windows 10 WHLK.
- Updated the Microcode version to 0x1D.
- Added Tropo Pro VGA support.
- Added support for the 6-cell (PA5110U-1BRS) high capacity battery.
- Initial production release for these models.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.