Q300 Series SSD Firmware Update Tool
- File: SSD_Firmware_Up...
- Version: 1.0.1.4
- Posted Date: 2015-11-23
- Release Date: 2015-11-23
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
-
This tool will allow the user to update the firmware on a Q300 Series (HDTS7xx) SSD.
For usage instructions see the following: Q300 Firmware Update Tool Instructions
NOTE: For Windows 7 users, application of Windows security update program(KB3033929) is required before updating Q300 Firmware.
https://www.microsoft.com/en-US/download/details.aspx?id=46148
The Q300 firmware update failure is caused by Windows driver issue. Microsoft has already released Windows security update program for the driver issue. After installing Windows security update, the Q300 firmware can be updated successfully.
If you received an inquiry related update failure, please confirm that the latest Windows update program applied to the PC first.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.