ConfigFree's Connectivity Doctor always reports that the Wireless Switch is off
- Document ID: 98081620
- Posted Date: 2005-05-23
- Last Updated: 2005-05-23
- Distribution: View Public Website
- Applicable Models
Satellite M30X-S1592ST Satellite M30X-S1593ST Satellite M30X-S171ST Satellite M30X-S181ST Satellite M30X-S191TD Satellite M30X-S221ST Satellite M30X-S221TD Satellite M35X-S109 Satellite M35X-S111 Satellite M35X-S114 Satellite M35X-S1141 Satellite M35X-S1142 Satellite M35X-S1143 Satellite M35X-S149 Satellite M35X-S1491 Satellite M35X-S1492 Satellite M35X-S161 Satellite M35X-S1611 Satellite M35X-S163 Satellite M35X-S1631 Satellite M35X-S309 Satellite M35X-S3091 Satellite M35X-S311 Satellite M35X-S3111 Satellite M35X-S3112 Satellite M35X-S329 Satellite M35X-S3291 Satellite M35X-S349 Satellite M35X-S3491
- Issue
ConfigFree Connectivity Doctor's icon for the wireless network antenna switch always indicates that the switch is OFF, whether it is actually set in the ON position or the OFF position.This is accompanied by a dialog box showing the switch being off as possible cause of a connection problem, with a possible solution being to turn the switch on. There may be no actual connection problem (you may be able to access websites and / or local network resources).
- Resolution
Use Control Panel's Add or Remove Programs utility to uninstall the Toshiba Hotkey Utility, and then reinstall it.This program is called E-Key Utility on the Toshiba Satellite M30X/M35X Recovery and Applications/Drivers DVD. It's called Toshiba E-Key Utility for Windows XP on the Toshiba Support website.
- Procedure
Unistalling the Toshiba Hotkey Utility:- Click Start.
- Click Control Panel.
- Double-click Add or Remove Programs.
- Select TOSHIBA Hotkey Utility.
- Click Change/Remove.
- Click OK to confirm that you wish to completely remove the selected application and its features. The InstallShield Wizard will begin the removal process.
- Click Finish to exit the InstallShield Wizard.
Re-installing the Toshiba Hotkey Utility using the Toshiba Satellite M30X/M35X Series Recovery and Applications/Drivers DVD that shipped with the computer:
- Insert the Toshiba Satellite M30X/M35X Series Recovery and Applications/Drivers DVD into the CD/DVD drive and close the tray. The setup program on the DVD should start automatically.
- When the Toshiba Recovery and Applications CD window appears, verify that "Install applications and drivers" is the selected install type, and click Next.
- Select E-key Utility from the list, and click Install.
- When the WinZip Self-Extractor window appears, click OK.
- Click Unzip.
- Click OK to acknowledge that the files were successfully unzipped.
- When the InstallShield window appears, click Next and follow the prompts to complete the installation.
- When the installation is complete, click Exit and then OK to close the Toshiba Recovery and Applications CD window.
- Remove the Toshiba Satellite M30X/M35X Series Recovery and Applications/Drivers DVD from the optical drive and close the tray.
Reinstalling the Toshiba Hotkey Utility using the file downloaded from the Toshiba Support website:
- Download the Toshiba E-key Utility for Windows XP from the Toshiba Support website, and save it to your computer. See also the bulletin Obtaining downloads and support docs from the Toshiba Support website.
- Navigate to where you saved the file and double-click it.
- Click Run.
- When the WinZip Self-Extractor window appears, click OK.
- Click Unzip.
- Click OK to acknowledge that the files were successfully unzipped.
- When the InstallShield window appears, click Next and follow the prompts to complete the installation.
- mm/wa
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.