Iomega Zip 250 USB Installations - Windows 95, 98, 98SE & Windows NT 4.0



Document ID: 98050519

 

Posted Date: 2000-02-18

 

Last Updated: 2000-01-20

 

Distribution: View Public Website

 

Applicable Models
Satellite 2065CDS
Satellite 2105CDS
Satellite 2510CDS
Satellite 2515CDS
Satellite 2535CDS
Satellite 2545CDS
Satellite 2595CDS
Satellite 2595CDT
Satellite 2595XDVD
Satellite 2655XDVD
Satellite 4030CDT
Satellite 4090XDVD
Satellite 4100XDVD
Portege 3025CT
Portege 3110CT
Portege 7010CT
Portege 7020CT
Tecra 8000
Tecra 8100

 

Issue
These are instructions for the Iomega Zip 250 USB Installations for Windows 95, 98, 98SE & Windows NT 4.0.
Procedure
Installation - Windows 95 w/Iomega USB

1.   Insert lomegaware v2.1 CD and it will AutoPlay. 
2.   Install Shield window opens and then the Windows Installer
       Window.
3.   Iomega Software Setup "Welcome to the Iomega Software Setup
       Wizard."  Click "Next."
4.   License Agreement screen - Select "I accept the terms" and
       click on "Next."
5.   Select "Complete" and click on "Next."
6.   Ready to Install the program, click on "Install."
7.   Iomega Software Setup screen - "Are you installing Iomega
       Software to support an Iomega USB drive?  Click on "Yes."
8.   Iomega Software Setup screen - 

       "IMPORTANT"  Windows 95 does NOT fully support the Universal
          Serial bus.  Once the Iomega USB drivers are installed,
          only Iomega devices will be supported on USB connections.
          
     Do you want to install the Iomega USB drivers?  Click on "Yes."
     Note: If you have, or are planning to install other USB devices,
       upgrade to Windows 98.  Windows 98 has full USB support.
9.   Completing the Iomega Software Setup screen - Select "Shut Down
       Now" and click "OK."
10.  Restart the computer.
11.  Iomega Software Setup screen states "No Iomega drives Detected."
       Click on "No."
12.  Select "Close this Window" and click "OK."
13.  The lomegaware program windows will be open. Leave open for now.
14.  Connect the USB cable to the Zip drive and then connect to USB
       port on computer.
15.  Plug the Zip drive AC adapter into power source and then to Zip
       drive.  New hardware will be detected.
16.  Restart computer.
17.  Iomega Software Setup screen -  'Here are the Iomega drives
       found on your system:
	 Zip 250 (x:).  "Are all of your Iomega drives listed?"
	 Click on "Yes."
18.  "Congratulations!  Installation is complete." screen.
        Click "OK."

     Installation is complete and the following will be listed in the
     Device Manager:
     
	Device Manager:
	
	Disk Drives:       Iomega Zip250
	SCSI Controllers:  Intel 82371AB/EB PCI to USB Universal Host
	                     Controller
	USB:               All devices and the USB category are removed.


Installing Zip 250 Card - Windows 95 & PC Card/Cable Option 
1.      Complete above installation instructions.
2.      Remove USB cable from computer’s USB connector.
3.      Remove USB Cable and AC Adapter from Zip 250 drive.
4.      Connect PC Card cable to Zip 250 drive.
5.      Insert PC Card into PCMCIA slot. 

        Installation is complete and the following will be listed in
        the Device Manager:
        
	Device Manager:
	
	Hard Disk Controllers:	Iomega Win98 USB Disk Controller
	                          changed to Zip PC Card Drive is
	                          added
	PCMCIA Socket:		PCMCIA Card Services is added
	USB Controller:		Iomega USB Mass Storage Class Driver
	                          is removed.

*********************************************************************

Installation - Windows 98B and Windows 98 Second Edition w/USB

1.     Insert lomegaware v2.1 CD and it will AutoPlay.
2.     Install Shield window opens and then the Windows Installer
         Window.
3.     Iomega Software Setup - "Welcome to the Iomega Software Setup
         Wizard."  Click "Next."
4.     License Agreement screen - Select "I accept the terms" and
         click on "Next."
5.     Select "Complete" and click on "Next."
6.     Ready to Install the program - click on "Install."  You will
         see several screens of file copying etc.
         
	    Note:  Units with NEC Open Host USB Controllers will
	      receive the following:
	      
	      "Warning: Setup has determined that there may be a
	      problem with your USB controller.  Data loss may result
	      if you use more than one USB device at the same time.
	      See the documentation that shipped with your drive or
	      cable for further details about your USB controller.
	    Click "OK" to continue copying files.
7.     Completing the Iomega Software Setup screen - Select "Shut
         Down Now" and click "OK."
8.     Restart the computer.
9.     Iomega Software Setup screen states "No Iomega drives
         Detected."  Click on "No."
10.    Select "Close this Window" and click "OK."
11.    The lomegaware program windows will be open.  Leave open for
         now.
12.    Connect the USB cable to the Zip drive and then connect to USB
         port on computer.
13.    Plug the Zip drive AC adapter into power source and then to
         Zip drive.  New hardware will be detected.  
14.    Restart computer.
15.    Iomega Software Setup screen - "Here are the Iomega drives
         found on your system:
	    Zip 250 (x:).  "Are all of your Iomega drives listed?"
	      Click on "Yes."
16.    "Congratulations!  Installation is complete." screen.  Click "OK."

       Installation is complete and the following will be listed in
       the Device Manager:
       
       DEVICE MANAGER
        
       SCSI Controllers:     **!Iomega Click! Parallel Port Interface
                                 (can be removed)
                             **!Iomega Parallel Port Zip Interface
                                 (can be removed)
       Disk Drives:          Iomega Zip 250
       Hard Disk Controllers:Iomega Win98 USB Disk Controller
       USB:                  Iomega USB Mass Storage Class Driver

       **Not installed on all units.
       
       
Installing Zip 250 Card - Windows 98 & PC Card/Cable Option

1.     Complete above installation instructions.
2.     Remove USB Cable and AC Adapter connectors from Zip 250 drive.
3.     Connect PC Card cable to Zip 250 drive.
4.     Insert PC Card into PCMCIA slot. 

	Installation is complete and the following will be listed
	in the Device Manager:
	
	Device Manager:
	Hard Disk Controllers:  Iomega Win98 USB Disk Controller
	                          changed to Zip PC Card Drive
	PCMCIA Socket:          PCMCIA Card Services
	USB Controller:         Iomega USB Mass Storage Class Driver
	                          is removed.

*********************************************************************

Installation - Windows NT Workstation 4.0 w/USB

1.      Insert lomegaware v2.1 CD and it will AutoPlay. 
2.      Install Shield window opens and then the Windows
          Installer Window.
3.      Iomega Software Setup - "Welcome to the Iomega Software Setup
          Wizard."  Click "Next."
4.      License Agreement screen - Select  'I accept the terms and
          click on  'Next. '
5.      Select "Complete" and click on "Next."
6.      Ready to Install the program - click on "Install."  You will
          see several screens of files copying, including a DOS
          window that will close on its own.
7.      Completing the Iomega Software Setup screen - Select "Shut
          Down Now" and click "OK."
8.      Shutdown Computer screen - Press the power button to turn
          computer off.
9.      Connect the USB cable to the Zip drive and then connect to
          USB port on computer.
10.     Plug the Zip drive AC adapter into power source and then to
          Zip drive 
11.     Restart computer.
12.     Iomega Software Setup screen - "Here are the Iomega drives
          found on your system:
	     Zip 250 (x:).  "Are all of your Iomega drives listed?"
	     Click on "Yes."
13.     "Congratulations!  Installation is complete." screen.  Click
           "OK."

	Installation is complete and the following will be listed in
	Control Panel:
	
	Devices:                     IOMEGNT
	                             iomusb
	                             
	SCSI Adapters:
	  Devices tab:	Iomega USB Driver For Mass Storage;
	                  Iomega Zip 250
	  Drivers tab:	Iomega Click! Parallel Port Interface
	                  (can be removed)
			Click! PC Card drive (can be removed)
			Jaz Jet PCI Driver (can be removed)
			USB Driver For Mass Storage (DO NOT REMOVE)
			ZIP Parallel Port/Jaz Traveler Driver
			  (can be removed)
	Services:       Iomega Access
			Windows Installer

* Zip 250 Card - Windows NT & PC Card/Cable Option
  The Zip 250 Card will not work with Windows NT.

*********************************************************************

ADDITIONAL COMMENTS:
Zip 250 Installations were completed on the following units:

2065CDS	   98     2105CDS   98SE
2515CDS    98     2535CDS   98 (Does not work with Windows 95)
2545XCDT   98     2595XDVD  98
2655XDVD   98SE   3025CT    98
3115CT     98     4030CDT   95,98, NT
4100XDVD   NT     3110CT    95, 98 (Does not work with NT)
4090XDVD   95,98  7010CT    95, 98, NT
7020CT     NT     8000      95, 98, NT
8100       98SE



                                                
Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.