Sony Battery Pack Recall Programs
- Document ID: 98082080
- Posted Date: 2006-10-10
- Last Updated: 2008-10-30
- Distribution: View Public Website
- Procedure
Programa de Reemplazo de Baterías
Updated October 30, 2008
Additional models added on October 30, 2008.
REPLACE YOUR BATTERY PACK TODAY.
Toshiba has determined that certain Sony battery packs installed in Toshiba portable computers have caused fires. Based on our investigation with Sony Corporation, we concluded that the battery cells in specific manufacturing lots could be affected and could result in a fire. In cooperation with the U.S. Consumer Product Safety Commission, we have elected to implement this battery pack replacement program, which is limited to specific manufacturing lots of the battery cells. Following the battery supplier’s recommendation, we are launching a new battery pack replacement program for affected battery packs.
Customers whose Toshiba portable computers contain the subject battery packs are eligible to receive a replacement battery pack free of charge.
We strongly recommend that customers participate in this new battery pack replacement program as soon as possible.
The subject battery packs will be replaced free of charge. This offer extends only to replacement of the subject battery packs, and does not include replacement of any Toshiba computer.
If you have an affected battery, you should stop using it immediately and remove it from your computer.
New computer and accessory models added on October 30, 2008:
COMPUTER MODELS ACCESSORY BATTERIES Satellite A70/A75 PA3383U-1BRS Satellite M30X/M35X PA3395U-1BRS Satellite M50/M55 PA3399U-1BRS Satellite P30/P35 PA3400U-1BRS Tecra A3 PA3421U-1BRS Tecra A5 Tecra S2 The computer and accessory battery models listed in the tables below are subject to earlier battery recall programs:

Computer Models Accessory Batteries Portege M300 **
Portege M400/M405 **
Portege S100/S105 **
Qosmio G35 **
Satellite A50 **
Satellite R10/R15 **
Satellite R20/R25 **
Satellite U200/U205 **
Tecra A2 **
Tecra M3 **
Tecra M4 **
Tecra M5 **
Tecra M6 **
Tecra M7 **
Tecra S3 **PA3191U-4BRS **
PA3191U-5BRS **
PA3356U-2BRS **
PA3356U-3BRS **
PA3475U-1BRS **
PA3476U-1BRS **
Computer Models Accessory Batteries Satellite A100/A105 ***
Tecra A7 ***PA3399U-2BRS ***
PA3451U-1BRS ***** Computer models added September 28, 2006
*** Computer models added July 18, 2007
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Toshiba end-user license agreement both of which you can view before downloading any such software.