Toshiba Windows 8 Upgrade Information
- Document ID: 98083978
- Posted Date: 2012-08-31
- Last Updated: 2012-08-31
- Distribution: View Public Website
- Procedure
Toshiba offers a premium support package for Microsoft’s exciting new Windows 8 Operating System. For assistance in upgrading or performing a new installation and training on how to maximize your use of your new Windows 8 Operating System, contact our Toshiba Expert care Team at 1-(855) 256-9005.
How to upgrade to Windows 8
Step 1: Check to see if your computer is supported by Toshiba for upgrade to Windows 8.
Select your 5 digit model part number from the list of supported models need help finding your model?
Your Model is supported by Toshiba for Windows 8 upgrade. Proceed to the following steps.You can find your 5 Digit Model Part Number located on the bottom of the laptop in the position indicated below

Step 2: Visit the Microsoft Compatibility Center for Windows 8 to see if your favorite apps and devices are compatible with Windows 8.
Step 3: View Information from Toshiba regarding any loss/limit of any features/functionality that may occur after your upgrade.
Step 4: Visit the Microsoft Windows 8 Upgrade offer web site to register and redeem your Windows 8 upgrade offer from Microsoft.
Step 5: Backup your data. If you need help click here or choose a Toshiba backup solution.
Step 6: Choose the type of Windows 8 installation and follow the instructions.
- Clean Install: Removes all programs and data files from your laptop, replacing them with a completely new installation of Windows 8
- Run the Windows 8 Upgrade that you redeemed from Microsoft in Step 4.
- Download, Install and Run the Toshiba Upgrade Assistant to guide you through the process of re-installing software and drivers.
- Upgrade install: Keeps Windows settings, personal files and applications.
- If your computer is purchased after Jun 1, 2012 then download, install and run the Toshiba Upgrade Assistant to guide you through the process of upgrading to Windows 8.
- If your computer is purchased between Jan 1 2011 and Jun 1 2012 then download the manual step-by-step instructions below.
- Download the manual Step-By-Step instructions to perform a Upgrade install below.
NOTE: You can use the Toshiba Upgrade Assistant after the Windows 8 upgrade to re-install Toshiba drivers and Software.
- Download, Install and Run the Toshiba Upgrade Assistant to guide you through the process of upgrading to Windows 8.
Download manual step-by-step custom "clean" install instructions.
Download manual step-by-step upgrade instructions.
NOTE: The manual step-by-step instructions include information from Toshiba regarding software, hardware, drivers or firmware required to perform an upgrade to Windows 8.
Windows 8 frequently asked questions
Windows 8 FAQs from Microsoft
Windows 8 FAQs from Toshiba
Toshiba Upgrade Assistant to simplify the Windows 8 installation process
The Toshiba Upgrade Assistant will guide you through upgrading your computer to Windows 8.
Download the Toshiba Upgrade Assistant
Download Toshiba drivers for Windows 8
Where to find individual software updates for Windows 8 installations on Toshiba laptops.
Where to find individual software updates for Windows 8 when using Toshiba Accessories (dynadock, external monitors and port replicators).
Windows 8 hardware and software requirements
Minimum Windows 8 hardware requirements:
- Processor: 1 gigahertz (GHz) or faster
- RAM: 1 gigabyte (GB) (32-bit) or 2 GB (64-bit)
- Hard disk space: 16 GB (32-bit) or 20 GB (64-bit)
- Graphics card: Microsoft DirectX 9 graphics device with WDDM driver
Additional requirements to use certain features:
- To use touch, you need a tablet or a monitor that supports multitouch.
- To access the Windows Store and to download and run apps, you need an active Internet connection and a screen resolution of at least 1024 x 768.
- To snap apps, you need a screen resolution of at least 1366 x 768.
For the latest information regarding hadrware or software requirements from Microsoft for Windows 8 visit the Windows 8 FAQ WEB page.
Toshiba has tested the following systems for upgrade to Windows 8
Click here for a complete list of tested systems that support an upgrade to Windows 8.
These tested systems do not support an upgrade to Windows 8: mini notebooks NB500, NB505, NB510, NB515 (model part numbers: PLL50 and PLL72)
- Clean Install: Removes all programs and data files from your laptop, replacing them with a completely new installation of Windows 8
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Toshiba end-user license agreement both of which you can view before downloading any such software.