Windows NT 4.0 Can't Create NTFS Partition over 4Gb During Install



Document ID: 94000557

 

Posted Date: 1996-08-19

 

Last Updated: 1996-08-19

 

Distribution: View Public Website

 

Applicable Models
Satellite 110CS
Satellite 110CT
Satellite 200CDS
Satellite 305CDS
Satellite 310CDS
Satellite 310CDT
Satellite 320CDS
Satellite 320CDT
Portege 300CT
Portege 320CT
Portege 610CT
Portege 650CT
Portege 660CDT
Tecra 500CDT
Tecra 500CS
Tecra 510CDT
Tecra 520CDT
Tecra 530CDT
Tecra 550CDT
Tecra 700CS
Tecra 700CT
Tecra 710CDT
Tecra 720CDT
Tecra 730CDT
Tecra 730XCDT
Tecra 740CDT
Tecra 750CDT
Tecra 780CDM
Tecra 780DVD
Satellite Pro 400CDT
Satellite Pro 400CS
Satellite Pro 415CS
Satellite Pro 425CDS
Satellite Pro 430CDS
Satellite Pro 430CDT
Satellite Pro 440CDT
Satellite Pro 440CDX
Satellite Pro 465CDX
Satellite Pro 470CDT
Satellite Pro 480CDT
Satellite Pro 490XCDT
libretto 100CT
Equium 5160D
Equium 5200D
Equium 5230D
Equium 6200D
Equium 6200M
Equium 6230D
Equium 6260M
Equium 7000D
Equium 7100D
Infinia 7130
Infinia 7160
Infinia 7161
Infinia 7200
Infinia 7201
Infinia 7202
Infinia 7230
Infinia 7231
Infinia 7260

 

Information

Windows NT 4 Can't Create An NTFS Partition over 4Gb During Installation


During the text based portion of the NT installation, it is possible to create and format partitions. The maximum size for an NTFS partition is very large (16 exabytes), however the maximum size for a FAT partition under NT is 4GB (2GB under DOS). If you format a partition as NTFS during NT installation, it originally formats it as FAT and then converts it in the final stages of the NT installation, and this you are limited to a maximum partition size of 4GB during the NT installation.

To get around this problem there are several paths of action open to you:

1. Before starting the installation,. insert the disk into an existing NT installation and partition/format the disk using Disk Administrator and then insert the disk into the machine to be installed 2.Partition the disk into smaller partitions, if you had a 5GB disk you could have a 1GB system partition, and a 4GB boot partition.

2. The system partition is the partition NT's core startup files are located, boot.ini, ntldr and ntdetect.com (ntbootdd.sys if SCSI), and will normally be the active partition. The boot partition is the partition that NT stores the rest of its files, i.e. the %systemroot% directory

3. Create a 4GB partition at installation time, and then extend the NTFS partition after installation has completed

4. Start Disk Administrator (Start - Programs - Administrative Tools - Disk Administrator)

5. Select the NTFS partition and holding down the Ctrl key select the unpartitioned space of the rest of the disk

6. From the Partition menu, select Extend Volume Set
Note - You cannot extend a NTFS partition if it is the boot or system partition (as the boot/system partition cannot be part of a volume set)


Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Toshiba end-user license agreement both of which you can view before downloading any such software.