Realtek Audio Driver



File: OS2014126A_TC00...




Version: 6.0.1.7195
 
Posted Date: 2014-04-01

 

Release Date: 2014-04-01

 

Package
WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
Description
This driver provides audio enhancements for your computer.

Change Points

  1. When installed in conjunction with DTS Studio Sound V1.1.45.0 or higher the following issue is resolved:
  2. Fixed: DTS function is disabled when repeatedly going into standby or hibernation while playing content.

Installation Instructions

  1. Save this file to a convenient location such as the Windows Desktop
  2. Save all work in progress and close open applications.
  3. From the Windows Desktop, run the downloaded file to start the installation.
    1. If a User Account Control or Open File message is displayed, press Continue.
    2. Press the Start button at the Toshiba Archive Extractor window.
    3. Follow the displayed instructions to complete the install.
    4. Restart the computer.

Driver Version Verification

  1. Open Control Panel.
  2. Select Programs and Features.
  3. Find Realtek Audio Driver.
  4. Verify that the driver version is 6.0.1.7195.
Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.