Toshiba HDD Accelerator
- File: OS2013443A_TC00...
- Version: 2.2.0000
- Posted Date: 2014-05-02
- Release Date: 2014-05-02
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
- This software accelerates the Hard Disk Drive (HDD) by using system memory as cache.
Change Points
- Modified so that an external HDD can be detected normally.
- Fixed: Blue screens after waking from a sleep state with a VHD connected to the computer.
Installation Instructions
- Save this file to a convenient location such as the Windows Desktop.
- Save all work in progress and close open applications.
- From the Windows Desktop, run the downloaded file to start the installation.
- If a User Account Control or Open File message is displayed, press Continue.
- Press the Start button at the Toshiba Archive Extractor window.
- Press the Next button at the InstallShield Wizard screen.
- Press the Finish button when the installation completes.
Driver Version Verification
- Open Control Panel.
- Select Programs - Uninstall a program
- Find TOSHIBA HDD Accelerator.
- Verify that the version is 1.2.0000.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.